Cannot see output from USB
Hello,
I have an STM32L4R5 MCU on a custom PCB and I have flashed it with my firmware via USB_OTG_FS. Both CubeProgrammer and the CubeIDE have worked in flashing the MCU for me, given I have an ST-LINK connected to it as well. I have USB_DM, VBUS_Sense, and USB_DP pins set up on my MCU. I am wondering how I can see some sort of output from my MCU. From my searching, I learned the DFU mode is only used for flashing and something like USB CDC is used for communication, through a serial port or UART. I am wondering some ways (preferably efficient and quick) I can go about seeing an output from my MCU that is running my firmware. If there needs to be any more clarification as to my wiring/setup, I will gladly add that. Can USB CDC be setup via firmware, or is it solely a hardware configuration? I do not have pins like UART/LPUART TX/RX connected on my MCU, however, they are able to be jumped of course. I have been using a NUCLEO development board to test my code. When connecting my MCU to CubeProgrammer via USB, I am not able to interact with things like SWV or the debugger which I have heard are able to show some sort of log details when the firmware is running. However, I am able to access SWV and Debug via the ST-LINK connection. I am completely new to this sphere and am learning alot.
Any advice or tips will help,
Thank you.