Capacitance of OSC_32 pins
Hello,
Datasheet DS14791 Rev 4 has a note on page 161 stating that PCB and pin capacitance for the OSC_IN/OSC_OUT Interface can be assumed as 4 pF combined.
I qoute: "For CL1 and CL2, it is recommended to use high-quality external ceramic capacitors,
designed for high-frequency applications, and selected to match the requirements of the
crystal or resonator (see Figure 20). CL1 and CL2 are usually the same size. The crystal
manufacturer typically specifies a load capacitance, which is the series combination of CL1
and CL2. The PCB and pin capacitance must be included (4 pF can be used as a rough
estimate of the combined pin and board capacitance)."
I would calculate C1 = C2 = 2*(C_LOAD - C_STRAY) and assume C_STRAY with 2 pF in this case.
- Can you confirm that this is the correct way to size C1 and C2?
I was wondering if the same assumption can be made for OSC32_IN and OSC32_OUT Pins. I didn't find a note on that. Otherwise I would go by the chapter 5.3.17 I/O port characteristics and assume 5 pF per pin.
- But since this a quite big difference to the 4pF combined from the note I assume that a similar assumption can be made for OSC32?
Best Regards
Lucas