Capacitor for VREF pin on SMT32L4P5CG MCU
Hi, I´m beginner in SMT32 MCU design, I´m doing a design for the above MCU and in the document "AN4555" that is for hardware develoment of these MCU series I founf that

So for my package (64 pins) the VREF and the VDDA power signals are bounded inside the MCU, and I only have the VDDA pin available on my package, then the AN4555 states that if the these power signals (VREF and VDDA) are internally bounded I need a 1uF capacitor on this pin, so in this case I need to place a capacitor on the VDDA pin?
And for another side if the decoupling recommedation for the VDDA pin is to place a 1uF it´s necessary to add another 1uF capacitor because on this pin (VDDA) there is the VREF power signal bonded internally?