Case STM32 ST-LINK Utility cannot connect Target
We purchased 403pcs MCUs (STM32F401VBH3) with date code 314 from Mouser website, as shown in the picture below, they have been assembled on the board,

When preparing to program them with ST-LINK utility and the programmer (ST-LINK/V2), I found that most of the MCUs could not be connected, and the utility interface said "Cannot connect Target", as shown below.

I have analyzed it and can rule out the following influencing factors
① Poor contact between the spring probes on the test jig and the test points on the board. (Note: Verified that the contacts are good )
② Poor contact between the programmer (ST-LINK/V2) and the connector (J3) on the PCBA. (Note: Verified that the contacts are good )
③ The operating voltage of MCU (STM32F401VBH3) is abnormal. (Note : Verified that the operating voltage is normal ,3.3V)
④ The peripheral components of MCU are abnormal. (Note : Verified that the peripheral components are normal )
I also tried to use “Connect under reset ” and select “ lower SWD frequency mode ” , as shown below, but the connect still failed and still showed “Cannot connect to target ”
.
However, we also have 98pcs MCUs (STM32F401VBH3) with date code 746, as shown in the picture below, they are also assembled on the same board, they can be successfully connected and can be successfully programmed.

Could you please tell me what is causing this problem and how I can fix it .
Thanks.