Skip to main content
Graduate
October 11, 2024
Solved

choose of a MCU

  • October 11, 2024
  • 2 replies
  • 765 views

Good morning.

I used the CUBEMX board selector because I wanted an MCU with many ADC. I chose the U family because it was written that it has 25 ADC and one CAN.

Jad_0-1728653026940.png

Unfortunately, I did not find these ADC while using the wizard. I only saw 3. how could i get more?

Capture d’écran 2024-10-11 à 15.26.59.png

best regards

 

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello,

    You are confusing the number of channels and the number of ADC instances.

    Each ADC has many ADC channels it could be up to 25 depending on the MCU part number.

    The number of ADC instances is provided in the datasheet:

    1 x 12 bit and 2 x 14-bit. The number of the channels depends on the package.

    SofLit_0-1728654732621.png

     

     

    2 replies

    mƎALLEmAnswer
    Technical Moderator
    October 11, 2024

    Hello,

    You are confusing the number of channels and the number of ADC instances.

    Each ADC has many ADC channels it could be up to 25 depending on the MCU part number.

    The number of ADC instances is provided in the datasheet:

    1 x 12 bit and 2 x 14-bit. The number of the channels depends on the package.

    SofLit_0-1728654732621.png

     

     

    Technical Moderator
    October 11, 2024

    But in CubeMx I think there is a mistake: ADC total (Converters) needs to be equal to 3.

    I'm getting back to you to confirm the issue.

    Internal ticket number for follow-up: 193535

    Technical Moderator
    December 2, 2024

    @mƎALLEm wrote:

    But in CubeMx I think there is a mistake: ADC total (Converters) needs to be equal to 3.

    I'm getting back to you to confirm the issue.

    Internal ticket number for follow-up: 193535


    Issue fixed in CubeMx V6.13.0.