Chosing FLASH for STM32H7
Hello Community,
According to data sheet of STM32H743VIT6 https://eu.mouser.com/datasheet/2/389/stm32h743vi-1760857.pdf
1) Dual mode Quad-SPI memory interface running up to 133 MHz
2) NOR/NAND Flash memory clocked up to 100 MHz in Synchronous mode
Q1: Is it possible run NOR/NAND Flash in Asynchronous mode?
Q2: Is it possible run NOR/NAND Flash, which has 120 MHZ (or 133 MHZ) Maximum Clock Frequency param?
Q3: Is it possible run NOR/NAND Flash on Quad-SPI memory interface?
Thanks.