Clarification on Debug Register Configuration in STM32H755
Hi,
I'm working with the NUCLEO-H755ZI-Q, which features dual cores (Cortex-M4 & Cortex-M7). I’m trying to understand whether these two cores have separate debug registers, such as DHCSR (Debug Halting Control and Status Register).
I have reviewed RM0399 and the Armv7-M Architecture Reference Manual, but I couldn't find a definitive answer. To investigate further, I attempted to access DHCSR (0xE000EDF0) on AP0 and AP3 using STM32CubeProgrammer, and I observed that both cores displayed the same value. However, when running a project in STM32CubeIDE, where I separately access DHCSR on M4 and M7, I see different values for each core.
This discrepancy has left me confused about the debug register configuration on STM32H755. Do Cortex-M4 and Cortex-M7 maintain independent debug registers, or are they shared?
Any insights or official documentation references would be greatly appreciated!