Question
Communicating in 16-bit parallel mode for Anybus module M40 connected to STM32F769 FMC interface issue
We are using a Any bus module M40 in our project which is based on STM32F769BI.
The FMC interface is connected to the Any-bus module as per the attached schematics. This interface works for 8-bit mode of anybus. However for 16-bit mode it is not working.I have attached the relevant code also. Want to know if any hardware or code corrections are needed to get this interface working.