Skip to main content
Visitor II
October 23, 2024
Question

configure clock to achieve datasheet MCU current consumption?

  • October 23, 2024
  • 2 replies
  • 1042 views

I have the NUCLEO-G431RB, and I am trying to measure the MCU current consumption in different operation modes and frequencies. I have connected a multimeter at JP6 (IDD) to monitor the current. The problem is when I set the frequency (f HCLK) as stated in the datasheet the readings I got are very different from the one in the datasheet. You can see in Figure 1 an example of what I did in configuring the clock trying to get similar values as in the datasheet in Figure 2.

Hussain_0-1729684445252.png

Figure 1

Hussain_1-1729684582168.png

the current value I got is 29mA.

I want to know exactly how I should configure the clock in a proper way to get the correct readings

 

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    October 23, 2024

    Hello @Hussain 

    Are you sure all peripherals are disabled, prefetch is of, cashe is of, debug is disactivated.... Also, you need to make sure that temperture is exactly 25°. 

    Best Regards.

    STTwo-32 

    HussainAuthor
    Visitor II
    October 27, 2024

    I did not activate any peripherals, also 'Cashe' ON and 'Prefetch' OFF as the datasheet states. I did set them both OFF and no changes happened.

    Could you show me in detail how can I set the MCU settings correctly?
    It is probably that I missed something that led to the wrong setup.

    Super User
    October 28, 2024

    @Hussain wrote:

    I have the NUCLEO-G431RB, and I am trying to measure the MCU current consumption in different operation modes and frequencies. I have connected a multimeter at JP6 (IDD) to monitor the current.


    Are you sure that excludes all current to other things on the board - eg, the ST-Link?

    Show the code you are using to perform this test - see the posting tips for instructions:

    https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228