Configuring a G431RBT6 with cubeMX and the reference manual - confusing at least
I just wanted to configure the board. I never thought, that i would need more than 10 minutes at the first function (3 pins - timer for hall sensors).
It takes quite a bit of investigation to figure out those connections. I just want to ask if i am right, and if there are some tips (tutorials) that can help me. This is the second STM32 i am going to set up for a (for me) bigger project.
I had some issue here finding "tim_ti1f_ed", but i found "tim_ti1_ed", and after some more looking the actual place in the bigger diagram. Is this right? Are there any tables with those "tim_ti1f_ed" names, that could help and make it easy to remember?

Edit: Edited by ST Moderator to add the right Labels.