Configuring OSPI in QSPI with Memory Mapped
I am trying to setup my STM32H725 to use serial RAM in memory mapped mode. The memory I am using is:
IS66WVS4M8ALL RAM Datasheet
I have used IOC to setup the OCTOSPI1 as a QSPI peripheral and mapped CS IO0/1/2/3 CLK from the uC to the RAM.
I have tried to firstly set the RAM for 4 pin access, then setup the cfg for read and write, finally enable the memory mapped mode. Though it does not work, in debug mode it typically crashes at some point.
I have modified the init for Octospi accordingly:
static void MX_OCTOSPI1_Init(void)
{
/* USER CODE BEGIN OCTOSPI1_Init 0 */
/* USER CODE END OCTOSPI1_Init 0 */
OSPIM_CfgTypeDef sOspiManagerCfg = {0};
/* USER CODE BEGIN OCTOSPI1_Init 1 */
/* USER CODE END OCTOSPI1_Init 1 */
/* OCTOSPI1 parameter configuration*/
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThreshold = 1;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MICRON;
hospi1.Init.DeviceSize = 25;
hospi1.Init.ChipSelectHighTime = 5;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 2;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = 0;
hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;
hospi1.Init.MaxTran = 0;
hospi1.Init.Refresh = 241;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.NCSPort = 1;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI1_Init 2 */
OSPI_RegularCmdTypeDef sCommand;
OSPI_MemoryMappedTypeDef sMemMappedCfg;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressMode = HAL_OSPI_ADDRESS_4_LINES;
sCommand.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_ENABLE;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_ENABLE;
sCommand.DQSMode = HAL_OSPI_DQS_ENABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.Address = 0;
sCommand.NbData = 1;
sCommand.DummyCycles = 0;
/* Command SPI to be in QSPI Mode */
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.Instruction = 0x35; //set to quad mode
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
HAL_OK)
{
Error_Handler();
}
uint8_t dummyData[] = {0,0,0,0};
if (HAL_OSPI_Transmit(&hospi1, dummyData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
HAL_OK)
{
Error_Handler();
}
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_4_LINES;
sCommand.DataMode = HAL_OSPI_DATA_4_LINES;
/* Configure write operations */
sCommand.OperationType = HAL_OSPI_OPTYPE_WRITE_CFG;
sCommand.Instruction = 0x38;
sCommand.DummyCycles = 0;
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
HAL_OK)
{
Error_Handler();
}
/* Configure read operations */
sCommand.OperationType = HAL_OSPI_OPTYPE_READ_CFG;
sCommand.Instruction = 0xEB; //QCmd, QIO, upto 104MHz
sCommand.DummyCycles = 6;
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
HAL_OK)
{
Error_Handler();
}
sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
/*Enable memory mapped mode*/
if (HAL_OSPI_MemoryMapped(&hospi1, &sMemMappedCfg) != HAL_OK)
{
Error_Handler();
}
volatile uint32_t *externalFlash = 0x90000000;
uint32_t val1 = externalFlash[0];
HAL_Delay(1);
uint32_t val2 = externalFlash[1];
HAL_Delay(1);
externalFlash[0] = 10;
HAL_Delay(1);
externalFlash[1] = 10;
HAL_Delay(1);
val1 = externalFlash[0];
HAL_Delay(1);
val2 = externalFlash[1];
HAL_Delay(1);
/* USER CODE END OCTOSPI1_Init 2 */
}