Configuring Two UCPD Ports with X-CUBE-TCPP on STM32G0B1
Hello,
I’d like to configure two UCPD ports on STM32G0B1 in STM32CubeMX. I’m working on a custom board with two TCPP03-M20 (dual role). However, I’ve noticed that STM32CubeMX seems to support configuring only a single UCPD interface. I’ve tried setting it up, but I can’t figure out how to make it work for both ports. Is it possible to configure both UCPD interfaces manually in the code, or am I missing something in CubeMX? Any guidance or examples would be greatly appreciated.
Thanks
Vladislav