Connect STM32F769I-Discovery to MATLAB/Simulink for PiL-Simulation
Hi guys,
I want to use the STM32F769I-Discovery for a PiL-Simulation in MATLAB/Simulink. As a serial connection I use a USB A to Micro B that is plugged in at the CN15 USB ST-link Port on the microcontroller.. The thing is that when I want to run my model in PiL it doesn't detect the STM32 controller. In the Model Configuration Parameters I checked the COM Port which is in my case COM5. I also installed the ST-Link Debug which is listed in the USB devices section on my device manager.
I am thankful for any piece of advice.