Connecting external memory with STM32H753ZIT6
Hello Team,
I need to connect following two devices with STM32H753ZIT6.
1. NAND Flash- MT29F64G08AFAA
2. RTC SRAM- DS1747WP-120IND+
Kindly review the attached schematics & let me know if any changes are required.
I am little worried about write protection pin (W/P# - pin 19) in NAND flash as there is no specific pin in FMC for it. so have connected it just with one of the I/O pin of STM controller.
same issue is with the RST# pin in RTC SRAM.
Thanks in advance.
Rohit