Correction Request: AN2867 Oscillator design
Rev 19 Page 16/59:

I believe this should read "increase" instead. The purpose of Rext is to limit the current and thus lower power dissipation in the crystal. So, lowering Rext increases power dissipation.
A separate issue is that this phrase is awkward at best. First of all, on many boards Rext=0. Since it certainly can't be any lower that that, it's a strange way of phrasing the issue to say that too low a value increases power dissipation. What the appnote is trying to say is that the value of Rext should be selected to meet two competing requirements: staying below Max Drive level (which may require increasing Rext), and having sufficient Gain margin (which via the resulting change in ESR, may require decreasing Rext).
CC @STOne-32