CubeMX does not reload correctly the ioc file if modifed offline
I have a project with its ioc, the setup of the peripherals are ok.
Now I want to edit a file while cubeide is closed and have the change reloaded when I reopen the ioc.
Let say that I set the baudrate of UART5 to 115200: in some file I'll have the UART5 init and in that function I'll have a line of code to set the baudrate to 115200:
huart5.Init.BaudRate = 115200;I was expecting that if I close the cubeide, change the code to:
huart5.Init.BaudRate = 57600;and then reopen cubemx it would load the new setting, but it seems that it does not.
Am I wrong to expect that behaviour or there is something going on here?
STM32CubeIDE
Version: 1.16.0
Build: 21983_20240628_1741 (UTC)