D+ PullUp Voltage Less
Hello Team,
Good Day !
Considering USB Specification , D+ line Pull-Up Should be high Once USB Connectors Plugs in , I Tried to Implement Following SCH to accomplish it.

3.3V Enabled through Transistor Q4 (MMBT2222ALT1G).
VBUS Signal Comes from Voltage Divider Network when USB Plugs in , See Below :

J14 is USB 2.0 Type B Connector.
Issue is When I plugged USB , Voltage Down to 2.5VDC from 2.8V @ L2 pin 4 ( i.e. D+ line). Ideally , It should be (3.3V- Vce ).
As per USB specs. It should be Minimum 2.8V on D+ pull up.
Device is : STM32F303
Regards,
Bhupendra