DAC (PA4) giving constant 2.4V in STM32F446RE
Hi,
Greetings!!
We have been using STM32F446RE MCU in the project. We have implemented the DAC in the application at pin PA4 and PA5. Both DACs are generating similar voltages for different application.
The PA4 DAC is connected to ADC of another MCU through a cable with 15 cm length. In few boards we have observed that this DAC at pin PA4 stops working and gives constant 2.4V. Whereas the DAC at pin PA5 works as expected. The DAC at pin PA5 is not connected anywhere at this moment.
What would be the reason for this situation. Kindly advise.
We have not used any protection circuit from PA4 of STM32 to ADC pin of other MCU. It is simply connected through a cable.
Thanks,
Purushottam