Data is not stored in the FIFO when FSEL is 1
What I want to do is send Write Enable instruction to external Flash and erase.
The environment is as follows.
Use Board : nucleo l4r5zi
IDE : Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a.(Version: 9.3.0)
FLASH : W25Q64JV
The connection diagram of the board and FLASH is shown below.

I want to send Write Enable instruction to 「W25Q64JV 2」.
The registers are set as follows.
●OCTOSPI

●OCTOSPIM

I send Write Enable instruction and then the Read Status instruction. 0 is always stored in the FIFO. (Of course I make sure the FTF is set before reading the data register)
I assume that the setting on the microcontroller side is wrong because when I check IO5 with an oscilloscope, I get the expected waveform.
For your information, when I set FSEL to 0 and communicated with 「W25Q64JV 1」 using IO0~IO3, the data was stored in the FIFO as expected.
If there are any settings that are missing, I would like to know.