DCMI affected due to enable the ICache and DCache in stm32h743
Hello,
I am using the STM32H743ZI2 controller with Cortex-M7 and firmware version 1.11.2 for a project where I am capturing camera data through DCMI and sending it over Ethernet using UDP to software that receives the data and builds a video stream.
However, I am facing an issue related to cache usage:
When I enable SCB_EnableICache() and SCB_EnableDCache(), the DCMI data is not being copied into the another buffer, resulting in the data being sent over Ethernet as zeros (00000000...). And the DCMI stops immediately capturing data.
example :---
while(HAL_DCMI_Start_DMA(&hdcmi,DCMI_MODE_CONTINUOUS(uint32_t)&Rx_B(uint32_t)320)!=HAL_OK){}
I Have Started the the dcmi and enter into while
while(1)
{
for(int i=0 ; i<1280 ; i++){
dcmi_temp[i] = Rx_B[i];
}
}
When I disable the I and D cache, the DCMI data is successfully copied into the another buffer, and the data is transmitted correctly. However, the Ethernet packet sending speed drops to 30-40 Mbps.(basically speed would be in 80 - 90 Mbps).
Could anyone provide insights on why the cache affects the DCMI data transfer and how to resolve this while maintaining higher Ethernet throughput?
i have uploaded EXAMPLE code in text document . plz check it and help me on this
Thank you in advance for your help!