Derivation of 12-character USB serial number in STM32C0's system bootloader
How does the bootloader in the STM32C071 system memory generate its 12-character USB serial number string descriptor (e.g. "205537C24236")? I notice some similarities between this serial number and the 96-bit unique device ID at address 0x1FFF7550, but overall they look very different. I'm asking because I would like my firmware to use the same serial number as the bootloader, and being able to use a compact serial number would be beneficial as well.
Here are some examples of the 96-bit unique ID (hex formatted, with dashes after every 2 bytes) and the corresponding 12-character USB serial number:
1: 7A00-2500-0150-3642-4837-3020, 205537C24236
2: 7B00-5700-0150-3642-4837-3020, 208737C34236
3: 7B00-2700-0150-3642-4837-3020, 205737C34236
4: 7B00-8100-0150-3642-4837-3020, 20B137C34236
I looked at the documentation of the unique ID in RM0490, section 30.1, but that documentation was partially incorrect and did not help.