didn't properly able to read and write of FMC_norflash @0x60000000

HI,
For testing and debugging FMC_norflash(MT28EW01aba) with custom h753 board, I used h743i-eval example as it is for read,write,erase, hence, i could read Manufactring code in memory browser, but in live expression i see address is different, so, where should i check for proper tx and rx data to be match.
#include "main.h"
#include "stm32h7xx_hal.h"
#include "stdio.h"
#define BUFFER_SIZE ((uint32_t)0x1000) // Buffer size for read/write operations
#define NOR_BANK_ADDR ((uint32_t)0x60000000) // Base address of the NOR flash
#define ERASE_TIMEOUT 0x00A00000U // Timeout for erase operation
#define PROGRAM_TIMEOUT 0x00001000U // Timeout for program operation
#define WRITE_READ_ADDR ((uint32_t)0x8000) // Address offset for read/write operations
#define MANUFACTURER_CODE ((uint16_t)0x0089) // Expected Manufacturer code
#define DEVICE_CODE1 ((uint16_t)0x227E) // Expected Device code 1
#define DEVICE_CODE2 ((uint16_t)0x2221) // Expected Device code 2
#define DEVICE_CODE3 ((uint16_t)0x2200) // Expected Device code 3
#define NOR_STATUS_READ_ID_ERROR 0x01 // Custom error code for read ID error
#define NOR_STATUS_ID_ERROR 0x02 // Custom error code for ID mismatch
/* Private variables ---------------------------------------------------------*/
uint16_t aTxBuffer[BUFFER_SIZE];
uint16_t aRxBuffer[BUFFER_SIZE];
__IO uint32_t uwWriteReadStatus = 0;
uint32_t uwIndex = 0;
NOR_HandleTypeDef hnor1;
NOR_IDTypeDef NOR_Id;
FMC_NORSRAM_TimingTypeDef NOR_Timing;
/* Private typedef -----------------------------------------------------------*/
typedef enum
{
FAILED = 0,
PASSED = !FAILED
} TestStatus;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
HAL_StatusTypeDef MX_FMC_Init(void);
void Error_Handler(void);
static void Fill_Buffer(uint16_t *pBuffer, uint32_t uwBufferLenght, uint16_t uwOffset);
static TestStatus Buffercmp(uint16_t *pBuffer1, uint16_t *pBuffer2, uint16_t BufferLength);
static void CPU_CACHE_Enable(void);
static void MPU_Config(void);
/* Main Program --------------------------------------------------------------*/
int main(void)
{
/* Enable CPU Cache */
CPU_CACHE_Enable();
/* MPU Configuration */
MPU_Config();
/* HAL Initialization */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize GPIO */
MX_GPIO_Init();
/* Initialize FMC (NOR flash) */
if (MX_FMC_Init() != HAL_OK)
{
Error_Handler();
}
/* Fill the buffer to write */
Fill_Buffer(aTxBuffer, BUFFER_SIZE, 0xD20F);
for (int i = 0; i < BUFFER_SIZE; i++) {
printf("aTxBuffer[%d] = 0x%X\n", i, aTxBuffer[i]);
}
/* Erase the NOR flash block */
if (HAL_NOR_Erase_Block(&hnor1, WRITE_READ_ADDR, NOR_BANK_ADDR) != HAL_OK)
{
Error_Handler();
}
/* Wait until NOR is ready */
if(HAL_NOR_GetStatus(&hnor1, NOR_BANK_ADDR, ERASE_TIMEOUT) != HAL_NOR_STATUS_SUCCESS)
{
Error_Handler();
}
/* Write data to the NOR memory */
for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++)
{
if (HAL_NOR_Program(&hnor1, (uint32_t *)(NOR_BANK_ADDR + WRITE_READ_ADDR + 2 * uwIndex), &aTxBuffer[uwIndex]) != HAL_OK)
{
Error_Handler();
}
/* Check the status after each write operation */
if(HAL_NOR_GetStatus(&hnor1, NOR_BANK_ADDR, PROGRAM_TIMEOUT) != HAL_NOR_STATUS_SUCCESS)
{
Error_Handler();
}
}
/* Read data back from NOR flash */
if(HAL_NOR_ReadBuffer(&hnor1, NOR_BANK_ADDR + WRITE_READ_ADDR, aRxBuffer, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
/* Checking data integrity */
uwWriteReadStatus = Buffercmp(aTxBuffer, aRxBuffer, BUFFER_SIZE);
if (uwWriteReadStatus != PASSED)
{
/* Toggle the LED connected to GPIOI Pin 8 to indicate an error */
while(1)
{
HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_8);
HAL_Delay(500);
}
}
else
{
// Optionally, indicate success by turning on an LED or similar
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_8, GPIO_PIN_SET);
}
/* Infinite loop */
while (1)
{
}
}
/* Helper Functions ----------------------------------------------------------*/
/* Function to fill the buffer with test data */
static void Fill_Buffer(uint16_t *pBuffer, uint32_t uwBufferLenght, uint16_t uwOffset)
{
uint16_t tmpIndex = 0;
/* Put in global buffer different values */
for (tmpIndex = 0; tmpIndex < uwBufferLenght; tmpIndex++ )
{
pBuffer[tmpIndex] = tmpIndex + uwOffset;
}
}
/* Function to compare two buffers */
static TestStatus Buffercmp(uint16_t* pBuffer1, uint16_t* pBuffer2, uint16_t BufferLength)
{
while (BufferLength--)
{
if (*pBuffer1 != *pBuffer2)
{
return FAILED;
}
pBuffer1++;
pBuffer2++;
}
return PASSED;
}
HAL_StatusTypeDef MX_FMC_Init(void)
{
FMC_NORSRAM_TimingTypeDef Timing = {0};
hnor1.Instance = FMC_NORSRAM_DEVICE;
hnor1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
hnor1.Init.NSBank = FMC_NORSRAM_BANK1;
hnor1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hnor1.Init.MemoryType = FMC_MEMORY_TYPE_NOR;
hnor1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hnor1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hnor1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hnor1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hnor1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hnor1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hnor1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hnor1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE;
hnor1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hnor1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
hnor1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
hnor1.Init.PageSize = FMC_PAGE_SIZE_NONE;
Timing.AddressSetupTime = 15;
Timing.AddressHoldTime = 15;
Timing.DataSetupTime = 255;
Timing.BusTurnAroundDuration = 15;
Timing.CLKDivision = 16;
Timing.DataLatency = 17;
Timing.AccessMode = FMC_ACCESS_MODE_A;
if (HAL_NOR_Init(&hnor1, &Timing, NULL) != HAL_OK)
{
Error_Handler();
}
/* Read & Check the NOR device IDs */
if (HAL_NOR_Read_ID(&hnor1, &NOR_Id) != HAL_OK)
{
/* NOR read ID Error */
return NOR_STATUS_READ_ID_ERROR;
}
/* Test the NOR ID correctness */
if ((NOR_Id.Manufacturer_Code != MANUFACTURER_CODE) ||
(NOR_Id.Device_Code1 != DEVICE_CODE1) ||
(NOR_Id.Device_Code2 != DEVICE_CODE2) ||
(NOR_Id.Device_Code3 != DEVICE_CODE3))
{
/* NOR ID not correct */
return NOR_STATUS_ID_ERROR;
}
printf("Manufacturer Code: 0x%X\n", NOR_Id.Manufacturer_Code);
printf("Device Code 1: 0x%X\n", NOR_Id.Device_Code1);
printf("Device Code 2: 0x%X\n", NOR_Id.Device_Code2);
printf("Device Code 3: 0x%X\n", NOR_Id.Device_Code3);
return HAL_OK;
}