Digital Input Wrong value
I have done a PCB Design with microcontroller STM32L071CZT6 as the mcu. PB15 which is a 5V tolerant pin is connected to a source of 4.9 V with a resistor 270 kOhm in between. I measured the voltage at the PB15 pin to be 4.9 V but, when I set it as Digital Input pin with no pull it does not read HIGH. But, I remember the previous batch of boards with the same design had this pin read HIGH by the same firmware.