DMA data alignment: zero-extension from 16-bit ADC to 32-bit memory on STM32H7
Hello,
I am working with an NUCLEO-H753ZI (ADC1/ADC2 with DMA1/DMA2, and ADC3 with BDMA).
My goal is to store ADC conversion results directly into a uint32_t buffer using DMA, so that the 16 valid bits from the ADC are automatically zero-extended to 32 bits in memory.
The reference manual describes the possible data widths (byte, half-word, word) for peripheral and memory sides, but I could not find a clear statement about what happens when:
-
Peripheral data alignment = half-word (16 bits)
-
Memory data alignment = word (32 bits)
Does the STM32H7 DMA (DMA1/DMA2 and BDMA) guarantee that the upper 16 bits are always zeroed when transferring 16-bit peripheral data into 32-bit memory? Or are the upper bits undefined?
In CubeMX, when configuring ADC1 or ADC2 with DMA, it is not possible to set MemDataAlignment=WORD in the .ioc file (the tool only allows HALFWORD). Is this a CubeMX limitation, or does it reflect a real hardware restriction?
Thanks in advance for your support!