Skip to main content
Graduate
October 21, 2024
Question

DMA does not work with ADC and TMR together.

  • October 21, 2024
  • 0 replies
  • 509 views

Hi, the device have some kind of limitation on the usage of DMA?

What I did:

1 - Implemented DMA0 stream 0 and 1 to do the following:

DMA0 stream 0 - Update the TMR2 ARR when TMR2overflow. Generate an Event on DMA transfer.

DMA0 stream 1 - Sync with the Event generated, Update the TMR3 ARR.

This worked fine.

2 - Implemented DMA0 stream 2 and 3 to do the following:

DMA0 stream 2 - Transfer data from ADC1 to Buffer.

DMA0 stream 3 - Transfer data from ADC2 to Buffer.

Both ADC are trigger by TMR3 overflow.

This worked fine.

 

3 - I tried to implement the tests above together, and it does not work, TMR stopped to be updated.

4 - What is stranger if that I tried to use DMA1 stream 0 and 1 for the ADC, but it also did not work.

 

There is known or is some mistake I did?

 

The workaround was to use the TMR2 overflow interrupt to update TMR2/TMR3, and let the DMA only for the ADC's.

The board is the NUCLEO-H723ZG.

Thank you.

 
    This topic has been closed for replies.