DMA latency
I working through issues on an STM32G4 where at times I'm not getting the reaction time from the DMA that I would like. I read AN2548, and it is a very helpful resource. However, I'm seeing slightly worse response times than AN2548 would suggest, and I'm wondering why. I set up a simple program to test latency, which is to set up a dma request generator that triggers off EXTI and sends a burst of on-off values to a GPIO. I've set the CPU to doing nops during this burst so that there is no bus contention. I found that the initial response takes about 11 cycles and the repeated values take 8 cycles each at 170 MHz, both with no jitter. It seems from AN2548 I should expect 6 cycles for each. In addition AN2548 suggests "The reasonable and recommended safety margin for this occasion is 50%, leaving one‑third of the total bus capacity in reserve". I'm wondering how to calculate this capacity. Is it 170e6/8 due to seeming 8 cycles per transaction?
uint32_t gpio_a_bsrr[2] = {2, 2<<16};
DMAMUX1_Channel0->CCR = 1; // req gen 0
DMAMUX1_RequestGenerator0->RGCR = 1 << DMAMUX_RGxCR_GPOL_Pos | 0 << DMAMUX_RGxCR_SIG_ID_Pos | 31 << DMAMUX_RGxCR_GNBREQ_Pos | DMAMUX_RGxCR_GE;
DMA1_Channel1->CMAR = (uint32_t)&gpio_a_bsrr;
DMA1_Channel1->CPAR = (uint32_t)&GPIOA->BSRR;
DMA1_Channel1->CNDTR = 2;
DMA1_Channel1->CCR = DMA_CCR_CIRC | DMA_CCR_DIR | DMA_CCR_EN | DMA_CCR_MINC | DMA_CCR_MSIZE_1 | DMA_CCR_PSIZE_1;