Skip to main content
Explorer
January 3, 2024
Question

DMA to BSRR Transfer - single signal error

  • January 3, 2024
  • 5 replies
  • 2381 views

Hello!

 

I am using the STM32F446RE Nucleo Board and succeeded in sending a signal chain via DMA to the GPIO Bank B, i.e. the BSRR register. 

 

The DMA trigger works very fine. However, one of the 8 signals is missing/not generated/skipped...

 

This is where I need help. I cannot figure out, why there is only one signal missing, "rw_pulse2", while all the others are generated correctly. (attached, a screenshot of the LA capture).


This are the macros defined by the CubeIDE: 

#define row_sel1_GPIO_Port GPIOB

#define row_sel2_Pin GPIO_PIN_2

#define row_sel2_GPIO_Port GPIOB

#define row_sel3_Pin GPIO_PIN_4

#define row_sel3_GPIO_Port GPIOB

#define row_sel4_Pin GPIO_PIN_5

#define row_sel4_GPIO_Port GPIOB

#define rw_pulse4_Pin GPIO_PIN_6

#define rw_pulse4_GPIO_Port GPIOB

#define rw_pulse3_Pin GPIO_PIN_7

#define rw_pulse3_GPIO_Port GPIOB

#define rw_pulse1_Pin GPIO_PIN_8

#define rw_pulse1_GPIO_Port GPIOB

#define rw_pulse2_Pin GPIO_PIN_9

#define rw_pulse2_GPIO_Port GPIOB

 

The ones I further defined:

#define SET_ROW_SEL1 (row_sel1_Pin)

#define SET_ROW_SEL2 (row_sel2_Pin)

#define SET_ROW_SEL3 (row_sel3_Pin)

#define SET_ROW_SEL4 (row_sel4_Pin)

#define SET_RW_PULSE1 (rw_pulse1_Pin)

#define SET_RW_PULSE2 (rw_pulse2_Pin)

#define SET_RW_PULSE3 (rw_pulse3_Pin)

#define SET_RW_PULSE4 (rw_pulse4_Pin)

 

#define RESET_ROW_SEL1 ((uint32_t)row_sel1_Pin << 16U)

#define RESET_ROW_SEL2 ((uint32_t)row_sel2_Pin << 16U)

#define RESET_ROW_SEL3 ((uint32_t)row_sel3_Pin << 16U)

#define RESET_ROW_SEL4 ((uint32_t)row_sel4_Pin << 16U)

#define RESET_RW_PULSE1 ((uint32_t)rw_pulse1_Pin << 16U)

#define RESET_RW_PULSE2 ((uint32_t)rw_pulse2_Pin << 16U)

#define RESET_RW_PULSE3 ((uint32_t)rw_pulse3_Pin << 16U)

#define RESET_RW_PULSE4 ((uint32_t)rw_pulse4_Pin << 16U)

 

And the function that is responsible for the pattern generation and the DMA transfer:

 

void write_memristor(uint32_t cycles) {

 

static uint32_t row_pattern[8];

 

row_pattern[0] = SET_ROW_SEL1 | SET_RW_PULSE1 | RESET_ROW_SEL4 | RESET_ROW_SEL2;

row_pattern[1] = RESET_ROW_SEL1 | SET_ROW_SEL2 | SET_RW_PULSE2 | RESET_RW_PULSE3;

row_pattern[2] = RESET_ROW_SEL2 | SET_ROW_SEL3 | SET_RW_PULSE3 | RESET_RW_PULSE4;

row_pattern[3] = RESET_ROW_SEL3 | SET_ROW_SEL4 | RESET_RW_PULSE1 | SET_RW_PULSE4;

row_pattern[4] = SET_ROW_SEL1 | RESET_ROW_SEL4 | RESET_ROW_SEL2 | SET_RW_PULSE1;

row_pattern[5] = RESET_ROW_SEL1 | SET_ROW_SEL2 | RESET_RW_PULSE3 | SET_RW_PULSE2;

row_pattern[6] = RESET_ROW_SEL2 | SET_ROW_SEL3 | SET_RW_PULSE3 | RESET_RW_PULSE4;

row_pattern[7] = RESET_ROW_SEL3 | SET_ROW_SEL4 | RESET_RW_PULSE1 | SET_RW_PULSE4;

 

// Start the DMA transfer

HAL_DMA_Start_IT(&hdma_tim1_up, (uint32_t)row_pattern, (uint32_t)&(GPIOB->BSRR),8);

HAL_TIM_Base_Start_IT(&htim1); // Start the timer with interrupt

HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1);

HAL_TIM_PWM_Start_IT(&htim2, TIM_CHANNEL_1);

TIM1->DIER |= TIM_DIER_UDE; // Set UDE bit (update DMA request enable)

}

 

Thanks a lot!

Cheers,

Ruan!

 

    This topic has been closed for replies.

    5 replies

    Technical Moderator
    January 3, 2024

    Are you sure that the SB46 jumper is open on your NUCLEO-F446RE?

    Regards
    /Peter

    Explorer
    January 3, 2024

    Hello Peter,

     

    both SB46 and SB52 are open, I just checked with a multimeter!

     

    Thank you!

    Ruan!

    Super User
    January 3, 2024

    Just - is this sequence intentional: pulse 4312 - pin 6789 ? (not: 4321 )

     

    AScha3_0-1704293676470.png

     

    Explorer
    January 3, 2024

    Hey AScha.3,

     

    the pinout was more or less arbitrary, as long as all the pins could fit in one GPIO Bank, in this case B. 

     

    Cheers!

    Super User
    January 3, 2024

    Toggling PB9 in software (i.e. without DMA) works?

    JW