Does anybody have working write routine for OSPI ? STM32H7 MX25LM51245G
I used this
BSP_OSPI_NOR_Write(uint8_t* pData, uint32_t WriteAddr, uint32_t Size) from
but what happens after executing write I cannot access the H7 chip anymore.
I have to connect Boot0 pin to 3.3V then I can erase the internal FLASH in Cube programmer.
and it works again
uint8_t BSP_OSPI_NOR_Write(uint8_t* pData, uint32_t WriteAddr, uint32_t Size)
{
OSPI_RegularCmdTypeDef sCommand;
uint32_t end_addr, current_size, current_addr;
/* Calculation of the size between the write address and the end of the page */
current_size = MX25LM51245G_PAGE_SIZE - (WriteAddr % MX25LM51245G_PAGE_SIZE);
/* Check if the size of the data is less than the remaining place in the page */
if (current_size > Size)
{
current_size = Size;
}
/* Initialize the adress variables */
current_addr = WriteAddr;
end_addr = WriteAddr + Size;
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = OCTAL_PAGE_PROG_CMD;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_16_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytes = 0x00;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesSize = HAL_OSPI_ALTERNATE_BYTES_8_BITS;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.Instruction = OCTAL_PAGE_PROG_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
/* Perform the write page by page */
do
{
sCommand.Address = current_addr;
sCommand.NbData = current_size;
/* Enable write operations */
if (OSPI_NOR_WriteEnable(&OSPINORHandle) != OSPI_NOR_OK)
{
return OSPI_NOR_ERROR;
}
/* Configure the command */
if (HAL_OSPI_Command(&OSPINORHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return OSPI_NOR_ERROR;
}
/* Transmission of the data */
if (HAL_OSPI_Transmit(&OSPINORHandle, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return OSPI_NOR_ERROR;
}
/* Configure automatic polling mode to wait for end of program */
if (OSPI_NOR_AutoPollingMemReady(&OSPINORHandle, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != OSPI_NOR_OK)
{
return OSPI_NOR_ERROR;
}
/* Update the address and size variables for next page programming */
current_addr += current_size;
pData += current_size;
current_size = ((current_addr + MX25LM51245G_PAGE_SIZE) > end_addr) ? (end_addr - current_addr) : MX25LM51245G_PAGE_SIZE;
} while (current_addr < end_addr);
return OSPI_NOR_OK;
}