Skip to main content
Graduate
March 25, 2024
Solved

Does NUCLEO-IKS01A1 support I3C? (with NUCLEO-H503RB)

  • March 25, 2024
  • 1 reply
  • 1314 views

Hi, 

I'm trying to check I3C protocol with NUCLEO-H503RB and IKS01A1.

I just followed below link for I3C. 

https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3C

And I can see that the master transmit the data but there is no ACK from the slave.(I've attached the scope shot).

I was trying to buy IKS01A3, but it was out of stock, so I just bought IKS01A1. Because it seems same IC. Is it okay?

I've also tried below example from the github, but result is same. 

https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H503RB/Examples/I3C

Please help me to find a way to check I3C.

 

 

 

 

 

    This topic has been closed for replies.
    Best answer by LukeJang522

    Thank you for reply. 

    I found reason because I set the clock 12500 Khz which is maximum.

    After I change it to 3000Khz which is recommended by that link. it works well. 

    Thank you anyway.  

    1 reply

    Technical Moderator
    March 29, 2024

    Hello @LukeJang522 ,

    Have you checked the below examples, which may help you?

    These examples use X-NUCLEO-IKS4A1A and X-NUCLEO-IKS01A3.

    For you information, the X-NUCLEO-IKS01A1 is Not Recommended for New Design as shown in this link.

    KDJEM1_0-1711712265338.png

    So, you can use this link to buy X-NUCLEO-IKS01A3.

    KDJEM1_1-1711712748838.png

    Thank you.

    Kaouthar

     

     

    LukeJang522AuthorAnswer
    Graduate
    March 29, 2024

    Thank you for reply. 

    I found reason because I set the clock 12500 Khz which is maximum.

    After I change it to 3000Khz which is recommended by that link. it works well. 

    Thank you anyway.