Does STM32F479 support USB High Speed without an external PHY controller?
I have spent a few days trying to select the correct MCU for a project and trying to minimise the need for external ICs For example, I need the STM32F479VI MCU to appear as a USB Full Speed (480 Mbps) device.
However, in CubeIDE, when I select USB-OTG-HS I get the following screen,

The manual says,

It mentions USB 2.0 high-speed + host controller + on-chip full-speed PHY
I think this will only work with an external USB 2.0 High-Speed PHY.
Are there any STM32F4 that have an internal USB 2.0 High-Speed PHY?
Regards,
Daniel