Does STM32H56xx 1MB device has extra memory for high-cycle data?
Hi,
I have this question because the reference manual states:
“When flash high-cycle data area on Bank1 is enabled, the code memory map is not continuous from Bank1 to Bank2 on 2M- and 512K-byte devices.”
So, does this mean that enabling high-cycle data sectors as EDATA on a 1MB device does not affect the code memory space, while on 2MB and 512KB devices, some sectors are reassigned for EDATA usage? If that’s the case, it seems like the 1MB device effectively has an extra 96KB of high-cycle data memory.
Snaku