Does STM32H7 support ISSI's OctalRAM ?
Hello, thank you for reading this post, sincerely hope to help answer questions.
The OSPI interface of STM32H735IGK6 is used to connect ISSI66WVO32M8DBLL to ISSI's PSRAM, which can read and write registers but cannot read and write memory. When configuring the register, it is found that the 24-26-bit MTYP[2:0]:Memory Type in the OCTOSPI device configuration register 1 (OCTOSPI_DCR1) register is controversial. According to the description in the manual, the MTYP[2:0] is shown in Figure 1, while the configurable options in cubemx are shown in Figure 2. Both have bias; Moreover, the following paragraph was found in file AN5050 which did not indicate that the general OSPI interface supports ISSI's PSRAM, please see Figure 3 below, so I would like to confirm whether STM32H7 supports ISSI's PSRAM (the general OSPI interface protocol is not hyperbus).If supported, what mode should this option (memory type) select? Thanks for your answer.

Figure 1

Figure 2

Figure 3