Does STM32H7R7 LTDC support DE mode only?
Hi,
I am evaluating the STM32H7R7Z8J6, intended to working with a TFT-LCD which is working in parallel RGB interface with DE mode only. The HSYNC and VSYNC signals are not connected.
Both AN4861 (Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs) and RM0477 (STM32H7Rx/7Sx Arm®-based 32-bit MCUs) documents only SYNC+DE mode, but the does not mention if the DE-mode-only is supported or not? Could you help to point out the documentation where explains how the LTDC working for DE mode in detail?
Thanks!
Leo