edge-blanking with 3-phase center-aligned PWM
Hello,
Comparator in STM32G4 is very fast. some glitch which is detected by COMP (during commutation PWM).
The overcurrent detection using internal comparator triggers below the theory (40A insteand 100A for example) I'm having trouble implementing the blanking mode in COMP with 3 timers (1 for each phase) .
Do you have an example or a note application to implement this mode?
thanks in advance.