Efficient Method to Generate a Sine Wave Using DMA and TIM1
Hi
What is the most efficient method in program logic to generate a sine wave using an H-bridge with an advanced timer?
I am using TIM1 on an STM32 microcontroller, which has two channels (Channel 1 and Channel 2) and complementary outputs. For generating the sine wave, I am using the following configuration:
- Positive Half-Cycle: The MOSFETs Q1 and Q4 are driven with PWM signals, while Q2 and Q3 are turned off.
- Negative Half-Cycle: The MOSFETs Q2 and Q3 are driven with PWM signals, while Q1 and Q4 are turned off.
I am also using center-aligned mode. What is the best and most efficient method in program logic to achieve this?
I need programming logic on how to efficiently feed a sine wave to CCR1 and CCR2 via DMA to achieve this. What is the best method?
Can I feed a full sine wave array value using a single array (look up table )? or should each half-cycle be fed sequentially? Specifically, should the first half-cycle be fed, and then the polarity of the channels be inverted to handle the next half-cycle? What is the most efficient and straightforward way to achieve this?