elf has a LOAD segment with RWX permissions when using .RamFunc function
I've seen other posts to resolve the compiler warning of "elf has a LOAD segment with RWX permissions", but I'm receiving this warning only when calling functions in RAM using the .RamFunc segment attribute.
From the map file I've verified the function is being loaded into RAM. I could disable the warning, but would like to understand the underlying issue.
I'm working with the latest STMCubeIDE version 1.16.0, but also saw this in 1.15.0. I'm building code for the STM3H735 and STM32H745 families.