Enable PWM Output Channel with HAL like formally done with LL_TIM_CC_EnableChannel
I have an older code where I use TIM1 in PWM2 mode to generate a frequency for a buzzer connected to the OC Channel4. Code is coming from F051 project.
Now I started a new project and wanted to reuse the same principal, but i do not see the function to turn on an off the Output pin to get either low, or a the PWM signal on the output.
I was using LL_TIM_CC_EnableChannel (TIM3,LL_TIM_CHANNEL_CH4);
I found TIM_CCxNChannelCmd(&htim1, Channel, TIM_CCxN_ENABLE) in the HAL but this is static, so not intended to be used by my code.
What is the equivalent function for LL_TIM_CC_EnableChannel in the HAL ?