Erasing memory corresponding to segment 0: Erasing internal memory sectors [0 150] Error: failed to erase memory
Hi
. I am using STM32L010C6tx processor. I drew the circuit myself. I did SYS-> debug serial wire. I was able to install without any problem. But sometimes "Memory Programming...
Opening and parsing file: ST-LINK_GDB_server_a14408.srec
File : ST-LINK_GDB_server_a14408.srec
Size: 19268 Bytes
Address: 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 150]
Error: failed to erase memory
Error: failed to erase memory
ST-LINK device status: UNKNOWN
CM3 Failed to print all registers
FAILED to REGISTER Values from the target
Debugger connection lost.
Shutting down...
" I'm getting it. I can't fix it. Any ideas?