errata: your ADC sample time in both the User Manual and CubeMx is wrong/misleading
I'm using STM32CubeMX 5.3.0, and RM0410 Rev 4.
RM p450 says
T_conv = Sampling time + 12 cycles.
This is wrong/misleading. Actually, this is the truth:
T_conv_total = Sampling time + T_conv_at_a_given_resolution,
The converstion times at a given resolution are described under Section 15.7: Fast conversion mode. They are:
T_conv_at_a_given_resolution:
12 bits --> 12 clock cycles
10 bites --> 10 clock cycles
8 bites --> 8 clock cycles
6 bits --> 6 clock cycles
Notice the pattern here: 1 clock cycle per bit of resolution.
Please fix RM p450 to clarify this.
RM p452 (15.7 Fast conversion mode) is also wrong/misleading.
It says that 12 bits takes 3 + 12 = 15 ADCCLK cycles. What is misleading is the 3. This is only if you have 3 set as your sample time! (see registers p473-474 for the sample times you can choose).
So, instead of RM p452 having this table ONLY:
• 12 bits: 3 + 12 = 15 ADCCLK cycles
• 10 bits: 3 + 10 = 13 ADCCLK cycles
• 8 bits: 3 + 8 = 11 ADCCLK cycles
• 6 bits: 3 + 6 = 9 ADCCLK cycles
It should have this table FIRST, followed by the above table, and with clarity added that the above table is for a sample time of 3 clock cycles.
• 12 bits: sampling_time + 12 ADCCLK cycles
• 10 bits: sampling_time + 10 ADCCLK cycles
• 8 bits: sampling_time + 8 ADCCLK cycles
• 6 bits: sampling_time + 6 ADCCLK cycles
STM32CubeMX propagates this erroneous and misleading information, as shown here:

It shows, for example: "12 bits (15 ADC Clock cycles)", which as I have just shown is MISLEADING. It should instead say, "12 bits (12 clock cycles + user-selected Sampling Time)", which makes a whole lot more sense and adds much clarity.
Here's some more screenshots to support what I'm saying.
From RM0410 450:

and p452:

and p473:

In short, please fix RM p450 and 452, and the CubeMx menu.
I suspect all other Reference Manuals for all other chips are affected similarly, so please look into all chips you make. Thanks.
Related:
Here's an answer I wrote about ADC sample time. That answer cross-links back to this post: https://electronics.stackexchange.com/questions/311326/stm32f20x-adc-sampling-time-rate/452200#452200.