Skip to main content
Visitor II
January 30, 2024
Solved

Error:Flash Download failed - "cortex-M4"

  • January 30, 2024
  • 3 replies
  • 7135 views

         Issue Description:  My code is divided into two parts, namely the APP area and the TRIM area. When I merge the code of these two areas together, there is no problem with programming through Keil. However, when I separate the code for these two areas (with the APP area located in the middle of Flash and the TRIM area at the end of Flash), the programming process results in an error (see Figure 1). My project configuration is shown in Figures 2 and 3.

        Phenomenon Description:  It's worth noting that this issue has not occurred on my computer but rather on a colleague's computer. I have attempted to troubleshoot by replacing the development board and using a different ST LINK on my colleague's computer, but the error persists.

      Platform Environment:

  1. Keil Version: V5.36.0.0
  2. Microcontroller (MCU): STM32L451CEUx
  3. Programmer: ST_LINK

 

LuckyDog_0-1706585535131.png

(Figures 1)

LuckyDog_1-1706585576869.png

(Figures 2)

LuckyDog_2-1706585576871.png

(Figures 3)

     Can you please advise on the cause of this error and how I can resolve it?

    This topic has been closed for replies.
    Best answer by Lucky Dog

    I found that the problem should be caused by different versions of the STM32L4xx_512.FLM file. The version installed on my computer is 2.6.2, and the version installed on my colleague's computer is lower than this version

     

    未命名图片.png

    3 replies

    Technical Moderator
    March 29, 2024

    Hi @Lucky Dog ,

    Could you please try the following:

    • perform the ST-Link Firmware upgrade
    • try to connect using the STM32CubeProgrammer and erase flash content before using Keil again

    -Amel

    Graduate II
    March 29, 2024

    What exactly does the pop-up error say when failing?

    Check the Keil website, I think there is an updated ST-LINK driver/dll

    Check power and VCAP situation. These could make the flash fail.

    Have Keil generate a .HEX file, try programming that with STM32 Cube Programmer.

    Lucky DogAuthorAnswer
    Visitor II
    October 12, 2024

    I found that the problem should be caused by different versions of the STM32L4xx_512.FLM file. The version installed on my computer is 2.6.2, and the version installed on my colleague's computer is lower than this version

     

    未命名图片.png

    Technical Moderator
    October 14, 2024

    Hi @Lucky Dog ,

    I assume that the latest version of Keil DFP package resolved the issue.

    Coming back to share your solution with the community after several months is well appreciated.

    -Amel