Skip to main content
Explorer
May 16, 2025
Solved

Error in RM0368 Reference manual, SPI Register Map is missing SPI_CR2 register

  • May 16, 2025
  • 1 reply
  • 376 views

Hello,

I noticed in the document RM0368 (Rev 6) for F401RE the SPI Register map (Table 93 page 611) is missing the SPI_CR2 register.

I came across this topic, created in 2021 and now closed :

https://community.st.com/t5/stm32-mcus-products/error-in-rm0368-reference-manual-spi-register-map-or-i-miss/m-p/225332

This topic was about Rev 5, and the problem should have been fixed in Rev 6.

 

Is my Rev 6 a too old document and it was patched in later revisions or is it still in the latest revisions as it appears that REV 6 is the latest version of RM0368 according to the F401RE product page :

https://www.st.com/en/microcontrollers-microprocessors/stm32f401re.html#documentation

Matt

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @MattGEII and welcome to the community;

     

    I confirm that rev6 is the latest revision of RM0368. Unfortunately the reported issue isn't yet fixed. I tracked it internally (210034) and I'll make sure to fix it.

    Internal ticket number: 210034 (This is an internal tracking number and is not accessible or usable by customers)

     

    Thank you.

    Kaouthar

    1 reply

    KDJEM.1Answer
    Technical Moderator
    May 19, 2025

    Hello @MattGEII and welcome to the community;

     

    I confirm that rev6 is the latest revision of RM0368. Unfortunately the reported issue isn't yet fixed. I tracked it internally (210034) and I'll make sure to fix it.

    Internal ticket number: 210034 (This is an internal tracking number and is not accessible or usable by customers)

     

    Thank you.

    Kaouthar