Skip to main content
Visitor II
October 10, 2024
Solved

Error in RM0490 Rev. 4 Section 6.2.6

  • October 10, 2024
  • 2 replies
  • 691 views

Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.

Should be the following:

Status bits in the RCC clock control register (RCC_CR) indicate which clock(s) is (are) ready.

Status bits in the RCC clock configuration register (RCC_CFGR) indicate which clock is currently used as a system clock.

    This topic has been closed for replies.
    Best answer by Simon.T

    Hello @MorganG ,

     

    I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

     

    Best regards,

     

    Simon

    2 replies

    Technical Moderator
    October 10, 2024

    Hello @MorganG and welcome to the Community,

    Thank you for raising this issue.

    I will check this and will get back to you soon with update (Internal ticket is submitted ID 193408 - not available outside of ST)

    Simon.TAnswer
    ST Employee
    October 10, 2024

    Hello @MorganG ,

     

    I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

     

    Best regards,

     

    Simon