Evaluation of Encoder Signal Level Shifting Approach
I’m working with an encoder that has a specification of 1024 pulses per revolution (p/r), and it will operate at a maximum speed of 1500 RPM. At this speed, the signal frequency produced by the encoder is approximately 25.6 kHz.
The encoder outputs a 5V signal, while my MCU (the STM32H743VIT6) can only handle a maximum input voltage of 3.3V. To address this, I plan to use a TXS0108E level shifter to convert the signal from 5V to 3.3V. Currently, I’m using a Blue Pill for testing until my main MCU arrives (the STM32H743VIT6).
I’d like to know if this is a good approach. Is the TXS0108E suitable for this application at the given frequency? Are there any better alternatives or recommendations for interfacing a 5V encoder output with a 3.3V MCU?
Thank you for your insights!