Skip to main content
Explorer
June 20, 2025
Solved

Exact allocation between propagation segment and phase segment 1

  • June 20, 2025
  • 1 reply
  • 262 views

Hello,

 

I am considering to use several STM32 microcontrollers to develop CANFD devices. I just saw CANFD Bosch specification v1.0, and more particularly scope 8 which defines the following requirements:

BBute1_0-1750420330453.png

Unfortunately, on all STM32 I have been confronted so far, you cannot specify exactly PROP seg and Phase seg 1 indivually but just the overall (Prop_seg+Phase_seg1). Which is fine to determine the sample point but I am not able to check if my bit timings are meeting the requirements above as I cannot discriminate prop seg length from phase 1 length.

1. Is the dispatch between propseg and phase seg 1 constant over all devices ?

2. Is the propagation segment always fixed to 1Tq for example ?

 

Any insight regarding this would be appreciated,

Best regards

 

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello,

    Hello for FDCAN timing, I propose you to refer to this Youtube video: FDCAN Normal Operating Mode

    Kvaser calculator can also help you for CAN-FD bit timing.

    Hope that helps.

    1 reply

    mƎALLEmAnswer
    Technical Moderator
    June 20, 2025

    Hello,

    Hello for FDCAN timing, I propose you to refer to this Youtube video: FDCAN Normal Operating Mode

    Kvaser calculator can also help you for CAN-FD bit timing.

    Hope that helps.