Excessive MCU heat after debugging
I have a design that uses two HRTIM outputs from an STM32G474 MCU to provide a PWM signal to two external half-bridge gate drivers to drive two DSMPS, a buck converter and an inverting buck-boost converter.
After several debugging sessions, the MCU continues to function but starts to heat for no apparent reason, exceeding 70°C and beyond, one time to destruction. The heating continues even if I erase the MCU with the STM32CubeProgrammer. After replacing the MCU, things are back to normal so it seems that I damaged the MCU while debugging. I'm still in the process of developing the control for the converters and am currently operating them open loop a fixed HRTIM PWM duty cycle to generate about +3V and -3V.
I've searched for, but could not find any reference to issues with debugging DSMPS. The biggest concern is the inverting buck-boost topology because if the HRTIM output is stuck high, +24V will get shorted through the pulse transformer, the top MOSFET, and the filter inductor to ground. Is it possible that during the process of updating the firmware via the debugger there can be a time that the HRTIM output is latched high? A clip from the schematic is below: