External clock requirement on N6 Family
Hello,
I was wondering about the reasons to supply external clocks to the N6 MCU, since it seems that via HSI and LSI there are clocks integrated into the MCU.
I am having trouble to understand whether the internal clocks can satisfy my requirements:
- I don't have special accuracy requirements for LSE/LSI nor HSI/HSE
- I am using the CSI-2 interface
- I am using SPI and UART Interface
Are there reasons to supply external clocks?
Are there other considerations that I might have to take into account? (especially for example considering data rates of the interfaces that I am using or other)
Best Regards
Lucas