External memory loader on STM32H7B0 with W25Q128 - can't select QSPI
Hi EveryOne,
I have made a custom board with STM32H7B0 and W25Q128 . where W25Q128 has to hold the user application . I hoped that i can change OSPI in STM32H7B0 to a QSPI config and work with W25Q128 ( which will only work with SPI or Qspi) . I can't able to select QSPI config ( which is mentioned as it is already activated ) in Octal SPI parameters . i'm using firmware version :FW H7 1.12.1

since this is a personal one i can't change the W25Q128 to another OSPI supported flash memory IC. Is there any example or any other way to make W25Q128 (changing OSPI to single SPI or using any one SPI communication) as a external memory to hold user application for STM32H7B0.