EXTI Edge Detection Characteristic for STM32H7 - rise/fall time?
I am trying to detect both rising and falling edges on a GPIO input using EXTI.
I am using a STM32H755 (144 pin) - SYSCLK is 400MHz, but I am using the CM4 core, so the CPU clock is 200MHz. APB Timer clock is also 200MHz.
The signal I am monitoring is coupled through an opto-isolator, and having scoped it, seems to have a rise-time of approx. 5us. I am wondering if this is too slow for EXTI rising / falling edge detection?
I've been looking at both the datasheet and reference guide for the STM32H755 and I could not find any data on max and min rise times for edge detection to function reliably.