Skip to main content
Visitor II
December 3, 2024
Solved

F407G-DISC1 RTC not working

  • December 3, 2024
  • 1 reply
  • 1131 views

I use F407G-DISC1 and RTC values dont change i have. In project i have I2S sound filtering and button that displays number on LEDs in binary, when button is pressed. But nothing happening on button press. Did i missed something?

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2019 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under Ultimate Liberty license
 * SLA0044, the "License"; You may not use this file except in compliance with
 * the License. You may obtain a copy of the License at:
 * www.st.com/SLA0044
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "filter_coef.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2S_HandleTypeDef hi2s2;
DMA_HandleTypeDef hdma_i2s2_ext_rx;
DMA_HandleTypeDef hdma_spi2_tx;
RTC_HandleTypeDef hrtc;

/* USER CODE BEGIN PV */
uint16_t mode=0;

RTC_TimeTypeDef RtcTime;
RTC_DateTypeDef RtcDate;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
void MX_RTC_Init(void);
static void MX_DMA_Init(void);
static void MX_I2S2_Init(void);

void GetTime(void);

uint16_t rxBuf[8];
uint16_t txBuf[8];

int Rand1;

static float firdata [FILTER_TAP_NUM];
static int firptr [FILTER_TAP_NUM];
static int fir_w_ptr=0;

static float firdata1 [FILTER_TAP_NUM1];
static int firptr1 [FILTER_TAP_NUM1];
static int fir_w_ptr1=0;

int main(void)
{
 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RTC_Init();
 MX_I2S2_Init();

 HAL_I2SEx_TransmitReceive_DMA (&hi2s2, txBuf, rxBuf, 4);

 while (1)
 {
	 if(mode == 0){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 1){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 2){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 3){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 4){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 5){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 6){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 7){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 8){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 9){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 10){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 11){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 12){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 13){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 14){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 15){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
 }
}

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	 //mode = mode + 1;
	 //if(mode > 3)
		// mode = 0;
	GetTime();
}

void GetTime(void)
{
	HAL_RTC_GetTime(&hrtc, &RtcTime, RTC_FORMAT_BIN);
	//mode = ((RtcTime.SecondFraction-RtcTime.SubSeconds)/((float)RtcTime.SecondFraction+1) * 100)/(125/8);//Rand1
	mode = RtcTime.Seconds/4;
	HAL_RTC_GetDate(&hrtc, &RtcDate, RTC_FORMAT_BIN);

}

int Calc_FIR (int inSample) {
	float inSampleF = (float)inSample;
	float outdata = 0;

	for (int i=0;i < FILTER_TAP_NUM; i++) {
		outdata += (firdata[i]*filter_taps[firptr[i]]);
		firptr[i]++;
	}

	firdata[fir_w_ptr] = inSampleF;
	firptr[fir_w_ptr] = 0;
	fir_w_ptr++;
	if (fir_w_ptr == FILTER_TAP_NUM) fir_w_ptr=0;

	return (int) outdata;
}

int Calc_FIR1 (int inSample) {
	float inSampleF = (float)inSample;
	float outdata = 0;

	for (int i=0;i < FILTER_TAP_NUM1; i++) {
		outdata += (firdata1[i]*filter_taps1[firptr1[i]]);
		firptr1[i]++;
	}

	firdata1[fir_w_ptr1] = inSampleF;
	firptr1[fir_w_ptr1] = 0;
	fir_w_ptr1++;
	if (fir_w_ptr1 == FILTER_TAP_NUM1) fir_w_ptr1=0;

	return (int) outdata;
}

int Calc_IIR_Left (int inSample) {
	float inSampleF = (float)inSample;
	float outSampleF =
			l_a0 * inSampleF
			+ l_a1 * lin_z1
			+ l_a2 * lin_z2
			- l_b1 * lout_z1
			- l_b2 * lout_z2;
	lin_z2 = lin_z1;
	lin_z1 = inSampleF;
	lout_z2 = lout_z1;
	lout_z1 = outSampleF;

	return (int) outSampleF;
}

int Calc_IIR_Right (int inSample) {
	float inSampleF = (float)inSample;
	float outSampleF =
			r_a0 * inSampleF
			+ r_a1 * rin_z1
			+ r_a2 * rin_z2
			- r_b1 * rout_z1
			- r_b2 * rout_z2;
	rin_z2 = rin_z1;
	rin_z1 = inSampleF;
	rout_z2 = rout_z1;
	rout_z1 = outSampleF;

	return (int) outSampleF;
}

void HAL_I2SEx_TxRxHalfCpltCallback(I2S_HandleTypeDef *hi2s){

	//restore signed 24 bit sample from 16-bit buffers
	int lSample = (int) (rxBuf[0]<<16)|rxBuf[1];
	int rSample = (int) (rxBuf[2]<<16)|rxBuf[3];

	// divide by 2 (rightshift) -> -6dB per sample
	lSample = lSample>>1;
	rSample = rSample>>1;

	//sum to mono
	lSample = rSample + lSample;

/*
	//run HP on left channel and LP on right channel
	lSample = Calc_FIR(lSample);
*/
	if(mode == 0)
		lSample = Calc_FIR(lSample);
	if(mode == 1)
		lSample = Calc_FIR1(lSample);
	if(mode == 2)
		lSample = Calc_IIR_Right(lSample);
	if(mode == 3)
		lSample = Calc_IIR_Left(lSample);

	//restore to buffer
	txBuf[0] = (lSample>>16)&0xFFFF;
	txBuf[1] = lSample&0xFFFF;
	txBuf[2] = (lSample>>16)&0xFFFF;
	txBuf[3] = lSample&0xFFFF;
}

void HAL_I2SEx_TxRxCpltCallback(I2S_HandleTypeDef *hi2s){

	//restore signed 24 bit sample from 16-bit buffers
	int lSample = (int) (rxBuf[4]<<16)|rxBuf[5];
	int rSample = (int) (rxBuf[6]<<16)|rxBuf[7];

	// divide by 2 (rightshift) -> -6dB per sample
	lSample = lSample>>1;
	rSample = rSample>>1;

	//sum to mono
	lSample = rSample + lSample;

	/*
	//run HP on left channel and LP on right channel
	lSample = Calc_FIR(lSample);
	 */
	if(mode == 0)
		lSample = Calc_FIR(lSample);
	if(mode == 1)
		lSample = Calc_FIR1(lSample);
	if(mode == 2)
		lSample = Calc_IIR_Right(lSample);
	if(mode == 3)
		lSample = Calc_IIR_Left(lSample);
	//restore to buffer
	txBuf[4] = (lSample>>16)&0xFFFF;
	txBuf[5] = lSample&0xFFFF;
	txBuf[6] = (lSample>>16)&0xFFFF;
	txBuf[7] = lSample&0xFFFF;
}


void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Configure the main internal regulator output voltage 
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSI;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON; //32 khz
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
 PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
 PeriphClkInitStruct.PLLI2S.PLLI2SN = 192;//96 kHz 192 -2,34% 197+0,23% 196-0,36%
 PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2S2 Initialization Function
 * None
 * @retval None
 */
static void MX_I2S2_Init(void)
{

 /* USER CODE BEGIN I2S2_Init 0 */

 /* USER CODE END I2S2_Init 0 */

 /* USER CODE BEGIN I2S2_Init 1 */

 /* USER CODE END I2S2_Init 1 */
 hi2s2.Instance = SPI2;
 hi2s2.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s2.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B;
 hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K;
 hi2s2.Init.CPOL = I2S_CPOL_LOW;
 hi2s2.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;
 if (HAL_I2S_Init(&hi2s2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2S2_Init 2 */

 /* USER CODE END I2S2_Init 2 */

}

/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
 /* DMA1_Stream4_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4, GPIO_PIN_RESET);

 /*Configure GPIO pin : PE3 */
 GPIO_InitStruct.Pin = GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pin : PC0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : PA0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PA4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PA5 PA6 PA7 */
 GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PB2 */
 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : PD12 PD13 PD14 PD15 
 PD4 */
 GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : PC7 PC10 PC12 */
 GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_10|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : PA9 */
 GPIO_InitStruct.Pin = GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PA10 PA11 PA12 */
 GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PD5 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : PB6 PB9 */
 GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : PE1 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI0_IRQn);
}

void MX_RTC_Init(void)
{
 RTC_TimeTypeDef sTime = {0};
 RTC_DateTypeDef sDate = {0};

 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }

 /* USER CODE BEGIN Check_RTC_BKUP */
 HAL_RTC_GetTime(&hrtc, &RtcTime, RTC_FORMAT_BIN);
 HAL_RTC_GetDate(&hrtc, &RtcDate, RTC_FORMAT_BIN);
 return;
 /* USER CODE END Check_RTC_BKUP */

 /** Initialize RTC and set the Time and Date
 */
 sTime.Hours = 19;
 sTime.Minutes = 50;
 sTime.Seconds = 12;
 sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sTime.StoreOperation = RTC_STOREOPERATION_RESET;
 if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }
 sDate.WeekDay = RTC_WEEKDAY_SATURDAY;
 sDate.Month = RTC_MONTH_MARCH;
 sDate.Date = 7;
 sDate.Year = 25;

 if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }

}

void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle)
{

 if(rtcHandle->Instance==RTC)
 {
 /* USER CODE BEGIN RTC_MspInit 0 */

 /* USER CODE END RTC_MspInit 0 */
 /* RTC clock enable */
 __HAL_RCC_RTC_ENABLE();
 /* USER CODE BEGIN RTC_MspInit 1 */

 /* USER CODE END RTC_MspInit 1 */
 }
}

void HAL_RTC_MspDeInit(RTC_HandleTypeDef* rtcHandle)
{

 if(rtcHandle->Instance==RTC)
 {
 /* USER CODE BEGIN RTC_MspDeInit 0 */

 /* USER CODE END RTC_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_RTC_DISABLE();
 /* USER CODE BEGIN RTC_MspDeInit 1 */

 /* USER CODE END RTC_MspDeInit 1 */
 }
}
/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */

 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{ 
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

 

 

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello,

    "still not working" does not bring much information as we don't have your environment. Tell what you tried to do to debug.

    "Break at address "0x8003b30" -> now forget about RTC and check your chip. Create a very simple project for example toggling a GPIO and find if you have the same issue.

     

    1 reply

    Technical Moderator
    December 3, 2024

    Hello,

    To find issues for a specific peripheral, try to simplify your code to focus on that issue. So remove all the code not related to the RTC and confirm if you have the same behavior.

    CzyzyKAuthor
    Visitor II
    December 3, 2024

    Hello,

    I removed I2S stuf, but still not working. Also i get "Break at address "0x8003b30" with no debug information available, or outside of program code."

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    RTC_HandleTypeDef hrtc;
    
    /* USER CODE BEGIN PV */
    uint16_t mode=0;
    
    RTC_TimeTypeDef RtcTime;
    RTC_DateTypeDef RtcDate;
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_RTC_Init(void);
    /* USER CODE BEGIN PFP */
    void GetTime(void);
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_RTC_Init();
     /* USER CODE BEGIN 2 */
    
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
    	 if(mode == 0){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 1){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 2){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 3){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 4){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 5){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 6){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 7){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
    	 if(mode == 8){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 9){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 10){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 11){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 12){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 13){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 14){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
    	 if(mode == 15){
    		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
    	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
     }
    }
    
    void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
    {
    	 //mode = mode + 1;
    	 //if(mode > 3)
    		// mode = 0;
    	GetTime();
    }
    
    void GetTime(void)
    {
    	HAL_RTC_GetTime(&hrtc, &RtcTime, RTC_FORMAT_BIN);
    	//mode = ((RtcTime.SecondFraction-RtcTime.SubSeconds)/((float)RtcTime.SecondFraction+1) * 100)/(125/8);//Rand1
    	mode = RtcTime.Seconds/4;
    	HAL_RTC_GetDate(&hrtc, &RtcDate, RTC_FORMAT_BIN);
    
    }
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     __HAL_RCC_PWR_CLK_ENABLE();
     __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.LSIState = RCC_LSI_ON;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
     RCC_OscInitStruct.PLL.PLLM = 8;
     RCC_OscInitStruct.PLL.PLLN = 50;
     RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
     RCC_OscInitStruct.PLL.PLLQ = 7;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief RTC Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_RTC_Init(void)
    {
    
     /* USER CODE BEGIN RTC_Init 0 */
    
     /* USER CODE END RTC_Init 0 */
    
     RTC_TimeTypeDef sTime = {0};
     RTC_DateTypeDef sDate = {0};
    
     /* USER CODE BEGIN RTC_Init 1 */
    
     /* USER CODE END RTC_Init 1 */
    
     /** Initialize RTC Only
     */
     hrtc.Instance = RTC;
     hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
     hrtc.Init.AsynchPrediv = 127;
     hrtc.Init.SynchPrediv = 255;
     hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
     hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
     hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
     if (HAL_RTC_Init(&hrtc) != HAL_OK)
     {
     Error_Handler();
     }
    
     /* USER CODE BEGIN Check_RTC_BKUP */
    
     /* USER CODE END Check_RTC_BKUP */
    
     /** Initialize RTC and set the Time and Date
     */
     sTime.Hours = 0x0;
     sTime.Minutes = 0x0;
     sTime.Seconds = 0x0;
     sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
     sTime.StoreOperation = RTC_STOREOPERATION_RESET;
     if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
     {
     Error_Handler();
     }
     sDate.WeekDay = RTC_WEEKDAY_MONDAY;
     sDate.Month = RTC_MONTH_JANUARY;
     sDate.Date = 0x1;
     sDate.Year = 0x0;
    
     if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN RTC_Init 2 */
    
     /* USER CODE END RTC_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOD_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
    
     /*Configure GPIO pin : PA0 */
     GPIO_InitStruct.Pin = GPIO_PIN_0;
     GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     /*Configure GPIO pins : PD12 PD13 PD14 PD15 */
     GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

     

    mƎALLEmAnswer
    Technical Moderator
    December 4, 2024

    Hello,

    "still not working" does not bring much information as we don't have your environment. Tell what you tried to do to debug.

    "Break at address "0x8003b30" -> now forget about RTC and check your chip. Create a very simple project for example toggling a GPIO and find if you have the same issue.