F767 CAN Bus issue
Hi,
I have an issue with the CAN1 controller in my MCU. I have connected the CAN transceiver to PA12(TX) and PA11(RX). When connected to the CAN Bus I can see the frames coming to the MCU(RX line) and the ACK bits are visible on the TX line. Unfortunately attempting to send any frame fails without any error in any of the registers.
After changing the TX Pin to PD1 everything runs smoothly. I did not apply any other changes in the parameters of the CAN controller in the CubeMX - just the pin change.
Any ideas for such behaviour?
Thanks.